Other Parts Discussed in Thread: HALCOGEN, DP83630
Using the LaunchXL2-RM57 and LwIP webserver application with CCS 9.3.0.00012.
In HALCoGen I have...
- GIO enabled on the Driver Enable tab
- GIOA enabled on the Pin Muxing tab
There is NO option for GIOA_4 to be mapped to ball A6.
On the LaunchXL2-RM57 ball A6 is used for GIOA_4 which connects to the RESET_N pin of the DP83630 PHY. A rather important pin to be able to control.