Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: Can i use nhet pin for another purpose?

Part Number: TMS570LC4357

Hi

I would like to ask for a piece of advice. I am dealing with an older PCB board with TMS570LC4357 on it. A new need for functionality appeared and i have a problem with NHET setting. I need to detect PWM signals with NHET2. But I also need to use some NHET2 pins as a simple output to maintain old functionality (it is cricial becaue there is located a reset signal to some periferies on the PCB). I figured out to run both functions but separately (PWM detector runs on NHET1). If NHET2 is enabled, simple output functionality is gone. (or at least for a moment. the periphery is reseted and then firmware shuts down everything.)

So my question is: Is it possible to enable NHET2 and to manage some outputs manually?

I hope i explained my self, thanks for reading.

Jan