Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

did jacinto 6 and cpsw driver can support avb ?

From the AVB point of view, just wanted to confirm if the support for the following is available in the cspw/ cpts driver and the switch IP on DRA7x.

  • IEEE 802.1BA:[4] Audio Video Bridging (AVB) Systems;
  • IEEE 802.1AS: Timing and Synchronization for Time-Sensitive Applications (gPTP);
  • IEEE 802.1Qat: Stream Reservation Protocol (SRP); and
  • IEEE 802.1Qav: Forwarding and Queuing for Time-Sensitive Streams (FQTSS).

and i want to know if i can run a simple_listener and talker with jacinto 6 board

thanks ,