This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux driver for ILI7807 TFT Driver IC.

FT055FHD-P01,RevA;191120.pdfHi,

I am using TFT LCD IC ILI7807. Can I get driver source code for this LCD module ? Can you suggest me,in Linux how to enable driver for this LCD module ?

This module includes GT9157 CTP Driver IC also. Can you suggest me how enable or add the driver for this in Linux ?

Attached the datasheet for reference.

Thanks and Regards,

Devendra

  • Hi Devendra,

    The part numbers you reference do not appear to be valid TI PNs. Do you have any questions related to TI devices or applications?

  • TFT/Linux Challenged Greetings,

    Perhaps more useful guidance sees you (initially) "Re-Directing your search to the (far more popular) Windows' based Code & Application Examples/Solutions."    (these are 'usually' supplied.)    Indeed these will not succeed under Linux - yet you should benefit from the "Source Code, Register based Parameters, and (even) critical code sequences."

    Armed w/that knowledge - your task simplifies & reduces to:

    • Taming Linux
    • Teasing the MCU into meeting the Display's Input Requirements

    Exercise care as (some) similar displays demand, "Multiple, Sequenced Power-Up (and Power-Down)" implementations!    The display's manual must be "Well-Read/Absorbed and you must comply w/its directives!"