Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: UNIFLASH, EK-TM4C1294XL
Hi,
I have just received some newly designed boards with TM4C1294 processors fitted. The issue is that the processors will program once and then there is no access to the processor through the SWD. I have used this processor on many designs without issue. My first instinct was to check the oscillator and this is not running. I have checked the load capacitors on the crystal they measure fine. I have no changed the crystal but have verified it is the correct part and oriented correctly There is no voltage on XOSC1 at all. Is there a way/steps to isolate the source of the problem.
In my design I have wake_n, OSC0 tied to GND and HIB_N is floating. Reset is functioning correctly 10K->3.3V 100n->GND. Any pointers would be appreciated.
Thanks,
Richard.