This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Supply current needed to power this device

Part Number: TMS570LS1224

Hello,

 I’m trying to select the current rating for the LDOs that will power the MCU (1.2V and 3.3V). What is the maximum current that I should consider for this LDO selection? I’m designing 2 versions of the board:

  1. MCU running UART or SPI --> For this, I want to use LDOs
  2. MCU running code to translate between CAN and UART and viceversa. --> For this, I’ll likely use a buck converter + LDOs.

I did review the supply current spec in the MCU datasheet, but it wasn't clear to me which spec to consider for these cases above. 

Best regards,

Leslie