Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
In the Halcogen tutorial example_sci_uart_9600.c there is a line meant to check if the SCI receiver is in idle state:
while ((UART->FLR & 0x4) == 4); /* wait until busy */
In this question, it is explained that it checks the BUSY bit of the FLR register: https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/839194/3103738?tisearch=e2e-sitesearch&keymatch=0x4%2520FLR#3103738
However, it is actually checking the IDLE bit of the FLR and not the BUSY bit. Can someone explain to me the difference between checking one bit and the other? The code works fine in both cases.
Thank you for your time.
Sergio