Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi,
Hi, I am integrating the DAC80508 with TMS570LC4357 controller. I am using Evaluation modules for both the chips. Connections are made according the description in the data sheet. The SPI 5 configured with 1 MHz clock (wanted to test with low clock speed initially). I have transmitted 24 bits (0x81 00 00) with 8 bit configuration in HalcoGen. I am facing issue with gaps between every 8 clock pulses. The slave is expecting continuous 24 bit clock pulses and the data to sync. How can I achieve this? Please help me.