Part Number: TMS570LC4357
Tool/software: Code Composer Studio
Hi,
When I load my program to the board I keep getting the error led ON. When I check the ESM register I'll get the following and the rest in 0.
If I press the Power reset button the led goes OFF.
What is this error related to? I don't understand very well; checking the TRF I see that when the Error key register is 5h -> The ERROR pin set to high when the low time counter (LTC) has completed; then the EKEY bit will switch back to normal mode (EKEY = 0000)
what should I do so that I don't get this error? and is the code correctly load?
Thanks and regards,
J