Part Number: TMDXRM46HDK
Tool/software: Code Composer Studio
Hi,
I'm trying to use F021 Flash API to erase the flash then load a new program.
1-) I copy some code on the RAM memory.
2-) I run this code to clear the flash.
void erase()
{
uint32_t s = 0;
Fapi_StatusType r = Fapi_initializeFlashBanks(128);
ENABLE_CPU_PRIVILEGE_MODE;
Fapi_FlashBankSectorsType type;
r = Fapi_getBankSectors(Fapi_FlashBank0, &type);
while (FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady);
s = FAPI_GET_FSM_STATUS;
r = Fapi_setActiveFlashBank(Fapi_FlashBank0);
r = Fapi_enableMainBankSectors(32);
while (FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady);
uint32_t* flash = (uint32_t*)(0x00014000);
r = Fapi_issueAsyncCommandWithAddress(Fapi_EraseSector, flash);
while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy );
do
{
s = FAPI_GET_FSM_STATUS;
}while(s != Fapi_Status_Success);
DISABLE_CPU_PRIVILEGE_MODE;
}
From the memory browser view, I can see that the memory for this banking sector is filled with 1.
3-) I try to write something in the flash
void program()
{
uint32_t s = 0;
Fapi_StatusType r = Fapi_initializeFlashBanks(128);
ENABLE_CPU_PRIVILEGE_MODE;
while (FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady);
s = FAPI_GET_FSM_STATUS;
r = Fapi_setActiveFlashBank(Fapi_FlashBank0);
r = Fapi_enableMainBankSectors(32);
while (FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady);
uint8_t tmp[8]={0};
r = Fapi_issueProgrammingCommand((uint32_t*)(0x00014000),
tmp,
8,
0,
0,
Fapi_AutoEccGeneration);
while( Fapi_checkFsmForReady() == Fapi_Status_FsmBusy );
do
{
s = Fapi_getFsmStatus(); //0x00001010
}while(s != Fapi_Status_Success);
DISABLE_CPU_PRIVILEGE_MODE;
}
Fapi_issueProgrammingCommand failed to write in the flash memory.
In FMSTAT register, PGV is set to 1.
The documentation states :
Program verify When set, indicates that a word is not successfully programmed after the maximum allowed number of program pulses are given for program operation.
I don't understand why writing fails.
Thanks