This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137-EP: ADC, Discharging both the sample cap and mux cap

Part Number: TMS570LS3137-EP


Please refer to SPNU499C section 19.11.53.  Question: when the sample cap inside the ADC is discharged is the 16 pF parasitic cap between the input mux and the sample switch also discharged.  The explanation for bit 0 in Table 19-58 of SPNU499C states that the internal sampling cap is connected to VREFLO.  It does not say what happens to Cmux.  Please refer to Figure 2 in TI document number SPNA118B for the location of Cmux.

Thank you,

John Colclough