Other Parts Discussed in Thread: SYSBIOS
Greetings
I m trying to communicate from my Connected LaunchPad TM4C1294 Tiva C Series Board with RN4678 with UART, but no matter what I do, I dont seem recive anything from the Bluetooth modul.
In the setup I m trying to reset and to toggle the RN4678 to make it UART ready, and I tested with an Oscilator if I do it right, and that should work.
The breaks inbetween are higher than in the documentation because there is just a minimum time which has to be reached before pulling the pins up.
Afterwards I try to get into command mode for the bluetooth modul but the modul which should return CMD to signal that it works doesnt come, my programm gets stuck at UART_read
Here is my code it looks very messy because i was trying everything to get it to work. Does someone of you have any idea what I do wrong? I use 120 MHz SysClock. I dont even know what information I could provide that would be usefull.
#include <stdbool.h>
#include <inc/hw_memmap.h>
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/Memory.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
/* TI-RTOS Header files */
#include <driverlib/sysctl.h>
#include <ti/drivers/UART.h>
/* Driverlib headers */
#include <driverlib/gpio.h>
#include <driverlib/pin_map.h>
/*Board Header files */
#include <Board.h>
#include <EK_TM4C1294XL.h>
/* Application headers */
#include "UART_Task.h"
#include "DebuggingMode.h"
//all commands end with carriage return '\r' '\x0d'
#define ENTER_COMMAND_MODE "$$$\r"
#define EXIT_COMMAND_MODE "---\r"
#define PARING_MODE "SM,6\r" //set remote address field SR
#define DEFAULT_MODE "SM,0\r"
#define SET_BLUETOOTH_MODE "SG,2\r"
#define ENABLE_UART "SH,1\r"
#define TURN_ON_DISCOVERY "W\r"
#define CONNECT_TO_DEVICE "C,0006668CB2A4\r"
#define SET_DEVICE_NAME "SN,SteuerungBoard\r"
#define DISPLAY_SETTING "D\r"
#define SET_BAUDRATE_19200 "SU,07\r"
/*
* ======== UART ========
* Echo Characters recieved and show reception on Port N Led 0
*/
void UARTFxn(UArg arg0, UArg arg1)
{
UART_Handle uart;
UART_Params uartParams;
/* Create a UART with data processing off. */
UART_Params_init(&uartParams);
uartParams.writeDataMode = UART_DATA_BINARY;
uartParams.readDataMode = UART_DATA_BINARY;
uartParams.readReturnMode = UART_RETURN_NEWLINE;
uartParams.readEcho = UART_ECHO_OFF;
uartParams.baudRate = 115200;
uartParams.dataLength = UART_LEN_8;
uart = UART_open(Board_UART2, &uartParams);
if (uart == NULL) {
System_abort("Error opening the UART");
}
uint32_t wait_ticks = (uint32_t) arg0;
// System_printf("CTS: %d", GPIOPinRead(GPIO_PORTP_BASE, GPIO_PIN_5));
// System_flush();
// while(GPIOPinRead(GPIO_PORTP_BASE, GPIO_PIN_5) != 0) {}
UART_write(uart, ENTER_COMMAND_MODE, sizeof(ENTER_COMMAND_MODE));
//UART_write(uart, DISPLAY_SETTING, sizeof(DISPLAY_SETTING));
memset(input, ' ', sizeof(input));
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_4, 0);
UART_read(uart, &input, MAXLEN);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_4, 1);
// UART_readPolling(uart, &input, MAXLEN);
System_printf("UART: %s \n", input);
System_flush();
/* Loop forever echoing */
bool needNew = true;
while (1) {
if(needNew) {
//UART_write(uart, '', sizeof(2));
UART_write(uart, ENABLE_UART, sizeof(ENABLE_UART));
needNew = false;
}
memset(input, ' ', sizeof(input));
UART_read(uart, &input, MAXLEN);
inputReady = true;
if(DEBUG){
System_printf("UART: %s \n", input);
System_flush();
}
UART_write(uart, DISPLAY_SETTING, sizeof(DISPLAY_SETTING));
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 1); // Remove this line to stop echoing!
Task_sleep(50);
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
//Return:
//$ššbš$GPRMC,193615.000,A,4818.6485,N,01634.1126,E,0.03,25.69,261219,,,D*58
//$GPV$GPRMC,193616.000,A,4818.6485,N,01634.1126,E,0.03,25.69,261219,,,D*5B
needNew = true;
Task_sleep(wait_ticks);
}
//TODO: exit command mode after finished communication
UART_write(uart, EXIT_COMMAND_MODE, sizeof(EXIT_COMMAND_MODE));
}
/*
* Setup task function
*/
// prio isnt used, wait_ticks isnt used, ui32SysClock is 120 000 000 Hz
int setup_UART_Task(int prio, uint32_t wait_ticks, uint32_t ui32SysClock) {
Task_Params taskUARTParams;
Task_Handle taskUART;
Error_Block eb;
//Setup Bluetooth module
//Wakeup PM7
// SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
// GPIOPinTypeGPIOOutput(GPIO_PORTM_BASE, GPIO_PIN_7);
// GPIOPinWrite(GPIO_PORTM_BASE, GPIO_PIN_7, GPIO_PIN_7);
//RST PP4
GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, GPIO_PIN_4);
// GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_4, GPIO_PIN_4);
//SW button low
//AN PD2
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_2);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2, 0);
System_printf("Pulling RST\n");
System_flush();
//Reset Pin Low
GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_4, 0);
// greater than 63 ns
SysCtlDelay(GPIO_PORTD_BASE*1);
//RST high
GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_4, GPIO_PIN_4);
SysCtlDelay(GPIO_PORTD_BASE*0.5);
System_printf("Setting SW_BTN High\n");
System_flush();
//BTN_SW High
//GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2, 0);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2, GPIO_PIN_2);
SysCtlDelay(GPIO_PORTD_BASE*2);
//Uart Handshake
//CTS RTS auf microcontroller PD4 auf output auf 0 wenn ich empfangen moechte
// GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_4);
//RTS CTS auf microcontroller PP5 auf input CTS ist auf 0 wenn ich schreiben kann
// GPIOPinTypeGPIOInput(GPIO_PORTP_BASE, GPIO_PIN_5);
/* Setup PortN LED1 activity signaling */
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART6);
GPIOPinConfigure(GPIO_PP0_U6RX);
GPIOPinConfigure(GPIO_PP1_U6TX);
GPIOPinTypeUART(GPIO_PORTP_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UART_init();
Error_init(&eb);
Task_Params_init(&taskUARTParams);
taskUARTParams.stackSize = 1024; /* stack in bytes */
taskUARTParams.arg0 = (UArg)wait_ticks;
taskUARTParams.arg1 = (UArg)"";
inputReady = false;
taskUARTParams.priority = prio; /* 0-15 (15 is highest priority on default -> see RTOS Task configuration) */
taskUART = Task_create((Task_FuncPtr)UARTFxn, &taskUARTParams, &eb);
if (taskUART == NULL) {
System_abort("TaskUART create failed");
}
return (0);
}