Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
This is the Device SPI register;
This is the halcogen part;
And the last one this is the code
#include "sys_common.h"
#include "sys_core.h"
#include "spi.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
uint16 TX_Data[] = {0xF7D0};
uint16 RX_Data[] = {};
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
spiDAT1_t dataconfig1_t;
dataconfig1_t.CS_HOLD = FALSE;
dataconfig1_t.WDEL = TRUE;
dataconfig1_t.DFSEL = SPI_FMT_0;
dataconfig1_t.CSNR = 0xFE;
spiInit();
spiSendData(spiREG1, &dataconfig1_t, 16, &TX_Data);
spiSendAndGetData(spiREG1, &dataconfig1_t, 16, &TX_Data, &RX_Data);
while(1)
{
};
/* USER CODE END */
return 0;
}
so nothing happen in the DAC part. Can anyone help me ?