Hello,
we are using all channels of ADC1 and ADC2. According to the datasheet (SPNS195C) , chapter 4.2.1.1 AD2IN[24] is routed to the pins V19 and W18. This is applicable for the 337ZWT package.
Questions:
1. Is AD2IN[24] mulitplexed to one of these pins?
2. How can I select the pin that shall be used for conversion?
In chapter 4.2.2.2 I cant find any information on mulitplexing for this signal.
Best regards
Markus