Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: Error while "NDK_hookInit() must be set in DSP/BIOS Task module config" manually configuring NDK

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

I'm trying to manually configuring and initiate the NDK stack using C code (as described in spru523k, section 2.1), but when I run my project I get this error in console:


00010.002 TaskGetEnv: FATAL: NDK_hookInit() must be set in DSP/BIOS Task module config (hookId == 0xffffffff)
00010.002 TaskSetEnv: FATAL: NDK_hookInit() must be set in BIOS Task module config (hookId == 0xffffffff)
00010.002 TaskGetEnv: FATAL: NDK_hookInit() must be set in DSP/BIOS Task module config (hookId == 0xffffffff)
Network Removed: d01a8c0
Network close hook!
ndkStackThread: exiting ...

Can anyone help me to solve this problem? I searched about it, but I couldn't solve it by myself.

Here is my stack initialization code:

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>

#include <ti/ndk/inc/netmain.h>
#include <ti/ndk/inc/os/oskern.h>
#include <ti/sysbios/knl/Clock.h>

#include <signal.h>
#include <time.h>

#include <xdc/std.h>
#include <xdc/runtime/System.h>

#include <ti/sysbios/utils/Load.h>

/* Socket file descriptor table */
#define MAXSOCKETS 10
uint32_t ti_ndk_socket_max_fd = MAXSOCKETS;
void *ti_ndk_socket_fdtable[MAXSOCKETS];

/* NDK memory manager page size and number of pages [used by mmAlloc()] */
#define RAW_PAGE_SIZE 3072
#define RAW_PAGE_COUNT 6

const int ti_ndk_config_Global_rawPageSize  = RAW_PAGE_SIZE;
const int ti_ndk_config_Global_rawPageCount = RAW_PAGE_COUNT;

/* P.I.T. (page information table) */
#ifdef __ti__
#pragma DATA_SECTION(ti_ndk_config_Global_pit, ".bss:NDK_MMBUFFER");
#pragma DATA_SECTION(ti_ndk_config_Global_pitBuffer, ".bss:NDK_MMBUFFER");
PITENTRY ti_ndk_config_Global_pit[RAW_PAGE_COUNT];
unsigned char ti_ndk_config_Global_pitBuffer[RAW_PAGE_SIZE * RAW_PAGE_COUNT];
#elif defined (__IAR_SYSTEMS_ICC__)
PITENTRY ti_ndk_config_Global_pit[RAW_PAGE_COUNT];
unsigned char ti_ndk_config_Global_pitBuffer[RAW_PAGE_SIZE * RAW_PAGE_COUNT];
#else
PITENTRY ti_ndk_config_Global_pit[RAW_PAGE_COUNT]
        __attribute__ ((section(".bss:NDK_MMBUFFER")));
unsigned char ti_ndk_config_Global_pitBuffer[RAW_PAGE_SIZE * RAW_PAGE_COUNT]
        __attribute__ ((section(".bss:NDK_MMBUFFER")));
#endif


/* --> ti_sysbios_knl_Task_hooks__A */
const __T1_ti_sysbios_knl_Task_hooks ti_sysbios_knl_Task_hooks__A[2];

/* --> NDK_hookInit */
extern xdc_Void NDK_hookInit(xdc_Int);
/* --> NDK_hookCreate */
extern xdc_Void NDK_hookCreate(ti_sysbios_knl_Task_Handle,xdc_runtime_Error_Block*);
/* --> NDK_hookExit */
extern xdc_Void NDK_hookExit(ti_sysbios_knl_Task_Handle);

/* --> ti_sysbios_knl_Task_hooks__A */
#pragma DATA_SECTION(ti_sysbios_knl_Task_hooks__A, ".const:ti_sysbios_knl_Task_hooks__A");
const __T1_ti_sysbios_knl_Task_hooks ti_sysbios_knl_Task_hooks__A[2] = {
    {
        ((xdc_Void(*)(xdc_Int))((xdc_Fxn)NDK_hookInit)),  /* registerFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle,xdc_runtime_Error_Block*))((xdc_Fxn)NDK_hookCreate)),  /* createFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))0),  /* readyFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle,ti_sysbios_knl_Task_Handle))0),  /* switchFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))((xdc_Fxn)NDK_hookExit)),  /* exitFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))0),  /* deleteFxn */
    },  /* [0] */
    {
        ((xdc_Void(*)(xdc_Int))((xdc_Fxn)ti_sysbios_utils_Load_taskRegHook__E)),  /* registerFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle,xdc_runtime_Error_Block*))((xdc_Fxn)ti_sysbios_utils_Load_taskCreateHook__E)),  /* createFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))0),  /* readyFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle,ti_sysbios_knl_Task_Handle))((xdc_Fxn)ti_sysbios_utils_Load_taskSwitchHook__E)),  /* switchFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))0),  /* exitFxn */
        ((xdc_Void(*)(ti_sysbios_knl_Task_Handle))((xdc_Fxn)ti_sysbios_utils_Load_taskDeleteHook__E)),  /* deleteFxn */
    },  /* [1] */
};


/* Memory bucket sizes */
#define SMALLEST 48
#define LARGEST (RAW_PAGE_SIZE)

const int ti_ndk_config_Global_smallest = SMALLEST;
const int ti_ndk_config_Global_largest  = LARGEST;

/* Memory Slot Tracking */
uint32_t ti_ndk_config_Global_Id2Size[] =
        {SMALLEST, 96, 128, 256, 512, 1536, LARGEST};

/*
 *  Local Packet Buffer Pool Definitions
 *
 *  The below variables/defines are used to override the defaults that are set
 *  in the Packet Buffer Manager (PBM) file src/stack/pbm/pbm_data.c
 */

/*
 *  Number of buffers in PBM packet buffer free pool
 *
 *  The number of buffers in the free pool can have a significant effect
 *  on performance, especially in UDP packet loss. Increasing this number
 *  will increase the size of the static packet pool use for both sending
 *  and receiving packets.
 */
#define PKT_NUM_FRAMEBUF 10

/* Size of Ethernet frame buffer */
#define PKT_SIZE_FRAMEBUF   1536

const int ti_ndk_config_Global_numFrameBuf = PKT_NUM_FRAMEBUF;
const int ti_ndk_config_Global_sizeFrameBuf = PKT_SIZE_FRAMEBUF;

/*
 *  Data space for packet buffers
 *
 *  Buffers are aligned on 4 byte boundaries to satisfy the EMAC's DMA
 */
unsigned char ti_ndk_config_Global_pBufMem[PKT_NUM_FRAMEBUF * PKT_SIZE_FRAMEBUF]
        __attribute__ ((aligned(4)));
unsigned char ti_ndk_config_Global_pHdrMem[PKT_NUM_FRAMEBUF * sizeof(PBM_Pkt)]
        __attribute__ ((aligned(4)));

/* Our NETCTRL callback functions */
static void networkOpen();
static void networkClose();
static void networkIPAddr(uint32_t IPAddr, uint32_t IfIdx, uint32_t fAdd);
static char *hostName = "tisoc";

extern void llTimerTick();

const char *LocalIPAddr = "192.168.1.13";
const char *LocalIPMask = "255.255.255.0";
const char *GatewayIP   = "192.168.1.1";
const char *DomainName  = "demo.net";

/*
 *  ======== networkOpen ========
 *  This function is called after the configuration has booted
 */
static void networkOpen()
{
    System_printf("Network open hook!\n");
    System_flush();
}

/*
 *  ======== networkClose ========
 *  This function is called when the network is shutting down,
 *  or when it no longer has any IP addresses assigned to it.
 */
static void networkClose()
{
    System_printf("Network close hook!\n");
    System_flush();
    // call user defined network close hook
}

/*
 *  ======== networkIPAddr ========
 *  This function is called whenever an IP address binding is
 *  added or removed from the system.
 */
static void networkIPAddr(uint32_t IPAddr, uint32_t IfIdx, uint32_t fAdd)
{
    //uint32_t IPTmp;

    if (fAdd) {
        //Display_printf(display, 0, 0, "Network Added: ");
        System_printf("Network Added: ");
    }
    else {
        //Display_printf(display, 0, 0, "Network Removed: ");
        System_printf("Network Removed: ");
    }
    System_printf("%x\n", IPAddr);
    System_flush();
}

/*
 *  ======== serviceReport ========
 *  Function for reporting service status updates.
 */
static char *taskName[] = {"Telnet", "HTTP", "NAT", "DHCPS", "DHCPC", "DNS"};
static char *reportStr[] = {"", "Running", "Updated", "Complete", "Fault"};
static char *statusStr[] = {"Disabled", "Waiting", "IPTerm", "Failed","Enabled"};
static void serviceReport(uint32_t item, uint32_t status, uint32_t report,
        void *h)
{
    System_printf("Service Status: %-9s: %-9s: %-9s: %03d\n",
            taskName[item - 1], statusStr[status], reportStr[report / 256],
            report & 0xFF);
    System_flush();
}

/*
 *  ======== initTcp ========
 *  Configure the stack's TCP settings
 */
static void initTcp(void *hCfg)
{
    int transmitBufSize = 1024;
    int receiveBufSize = 1024;
    int receiveBufLimit = 2048;

    CfgAddEntry(hCfg, CFGTAG_IP, CFGITEM_IP_SOCKTCPTXBUF, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&transmitBufSize, NULL);
    CfgAddEntry(hCfg, CFGTAG_IP, CFGITEM_IP_SOCKTCPRXBUF, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&receiveBufSize, NULL);
    CfgAddEntry(hCfg, CFGTAG_IP, CFGITEM_IP_SOCKTCPRXLIMIT, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&receiveBufLimit, NULL);
}

/*
 *  ======== initIp ========
 *  Configure the stack's IP settings
 */
static void initIp(void *hCfg)
{

    CI_SERVICE_DHCPC dhcpc;
    unsigned char DHCP_OPTIONS[] = { DHCPOPT_SUBNET_MASK };

    // hostname
    CfgAddEntry(hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_HOSTNAME, 0,
                strlen(hostName), (unsigned char *)hostName, NULL);

    // Usa DHCP para obter IP na interface 1
    memset(&dhcpc, 0, sizeof(dhcpc));
    dhcpc.cisargs.Mode = CIS_FLG_IFIDXVALID;
    dhcpc.cisargs.IfIdx = 1;
    dhcpc.cisargs.pCbSrv = &serviceReport;
    dhcpc.param.pOptions = DHCP_OPTIONS;
    dhcpc.param.len = 1;
    CfgAddEntry(hCfg, CFGTAG_SERVICE, CFGITEM_SERVICE_DHCPCLIENT, 0,
              sizeof(dhcpc), (unsigned char *)&dhcpc, NULL);

}

/*
 *  ======== initUdp ========
 *  Configure the stack's UDP settings
 */
void initUdp(void *hCfg)
{
    int receiveBufSize = 2048;

    CfgAddEntry(hCfg, CFGTAG_IP, CFGITEM_IP_SOCKUDPRXLIMIT, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&receiveBufSize, NULL);
}

/*
 *  ======== ndkStackThread ========
 *  NDK stack's main thread function
 */
void NDKManagerTaskFxn()
{
    void *hCfg;
    int rc;

    Clock_Params clockParams;
    Clock_Handle ndkClockHandle;

    // Create the NDK heart beat
    Clock_Params_init(&clockParams);
    clockParams.startFlag = TRUE;
    clockParams.period = 100;
    ndkClockHandle = Clock_create((Clock_FuncPtr)llTimerTick, clockParams.period,
                                  &clockParams, NULL);
    if (ndkClockHandle == NULL) {
        return;
    }

    rc = NC_SystemOpen(NC_PRIORITY_LOW, NC_OPMODE_INTERRUPT);
    if (rc) {
        return;
    }

    // create and build the system configuration from scratch.
    hCfg = CfgNew();
    if (!hCfg) {
        goto main_exit;
    }

    /* IP, TCP, and UDP config */
    initIp(hCfg);
    initTcp(hCfg);
    initUdp(hCfg);

    /* config low priority tasks stack size */
    rc = 2048;
    CfgAddEntry(hCfg, CFGTAG_OS, CFGITEM_OS_TASKSTKLOW, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&rc, NULL);

    /* config norm priority tasks stack size */
    rc = 2048;
    CfgAddEntry(hCfg, CFGTAG_OS, CFGITEM_OS_TASKSTKNORM, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&rc, NULL);

    /* config high priority tasks stack size */
    rc = 2048;
    CfgAddEntry(hCfg, CFGTAG_OS, CFGITEM_OS_TASKSTKHIGH, CFG_ADDMODE_UNIQUE,
            sizeof(uint32_t), (unsigned char *)&rc, NULL);

    do
    {
        rc = NC_NetStart(hCfg, networkOpen, networkClose, networkIPAddr);
    } while(rc > 0);

    CfgFree(hCfg);

main_exit:
    NC_SystemClose();

    System_printf("ndkStackThread: exiting ...\n");
    System_flush();
}

Thanks in advance,

Ronan