Part Number: TMS570LC4357
Hello,
I have a system, based on the I2C protocol, in which the TMS570LC4357 micro is acting as a slave. Now, depending on some user inputs, the master might want to send information to the slave (the TMS570LC4357 micro) at some point. In the meantime, the slave has to perform other tasks.
I am capable to send data and receive data with the master using i2cReceive and i2cSend when no interruptions are enabled. However, how can I set the slave to send data to the Master when I do not know when it is going to ask for it?
Checking the i2c interruptions in the reference manual, I do not see any type that could help me to solve this issue. I attach them here for commodity.