Other Parts Discussed in Thread: UNIFLASH
I am trying to jump from my bootloader to an application. I have two test application for this. One is a very simple while loop where a single variable keeps incrementing until it reaches 1000 and then gets reset to 0. Jumping to this application works, but when I use the pwmled2 example provided by the simplelink cc13x2 25x2 3.4 example I end up in the faultISR. I can see the PC being loaded with what should be the correct address, it then jumps to this address and when I go one step further using the debugger I end up in faultISR. I can not see what is happening at that address using the disassembly tool of Code Composer Studio because it just says Memory map prevented reading 0x001F1F1E.
I put the code I used on github in case someone want to give it a try: https://github.com/VincentKen/bootloader-cc2652. I upload the application over UART using a python script and the Intel Hex format.
This is the code I use to jump to the application:
void startApp(uint32_t sp) {
asm(" LDR SP, [R0, #0x0]");
asm(" LDR PC, [R0, #4]");
}
This is the test project that does work:
void main(void)
{
unsigned int test = 0;
while (1) {
test++;
if (test % 1000 == 0) {
test = 0;
}
}
}
This is the linker file of the bootloader:
--stack_size=1024 /* C stack is also used for ISR stack */
--heap_size=256
/* Retain interrupt vector table variable */
--retain=g_pfnVectors
/* Override default entry point. */
--entry_point ResetISR
/* Allow main() to take args */
--args 0x8
/* Suppress warnings and errors: */
/* - 10063: Warning about entry point not being _c_int00 */
/* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */
/* files compiled using Keil (ARM compiler) */
--diag_suppress=10063,16011,16012
#define FLASH_BASE 0x0
#define FLASH_SIZE 0x58000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x14000
#define GPRAM_BASE 0x11000000
#define GPRAM_SIZE 0x2000
#define FLASH_START FLASH_BASE
#define PAGE_SIZE 0x2000
#define BOOT_BASE 0x50000
#define BOOT_END CERT_START - 1
#define BOOT_SIZE ((BOOT_END) - (BOOT_BASE) + 1)
#define APP_BASE 0x0
#define APP_END BOOT_BASE
#define APP_SIZE BOOT_BASE
#define FLASH_CCFG_START 0x00057FA8
#define FLASH_CCFG_END (FLASH_START + FLASH_SIZE - 1)
#define FLASH_CCFG_SIZE ((FLASH_CCFG_END) - (FLASH_CCFG_START) + 1)
#define FLASH_FNPTR_START FLASH_CCFG_START - 8
#define FLASH_FNPTR_END FLASH_FNPTR_START + 3
#define FLASH_FNPTR_SIZE 4
#define CERT_END FLASH_FNPTR_START - 1
#define CERT_SIZE 0x4C
#define CERT_START CERT_END - CERT_SIZE + 1
/* System memory map */
MEMORY
{
BOOT (RX) : origin = BOOT_BASE, length = BOOT_SIZE
APP (RWX) : origin = APP_BASE, length = APP_SIZE
FLASH_CCFG (RX) : origin = FLASH_CCFG_START, length = FLASH_CCFG_SIZE
FLASH_FNPTR (RX) : origin = FLASH_FNPTR_START, length = FLASH_FNPTR_SIZE
FLASH_CERT (RX) : origin = CERT_START, length = CERT_SIZE
/* Application uses internal RAM for data */
SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
/* Application can use GPRAM region as RAM if cache is disabled in the CCFG
(DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
}
/* Create global constant that points to top of stack */
/* CCS: Change stack size under Project Properties */
__STACK_TOP = __stack + __STACK_SIZE;
/* Section allocation in memory */
SECTIONS
{
.intvecs : > BOOT_BASE
.text : > BOOT
.TI.ramfunc : {} load=BOOT, run=SRAM, table(BINIT)
.const : > BOOT
.constdata : > BOOT
.rodata : > BOOT
.binit : > BOOT
.cinit : > BOOT
.pinit : > BOOT
.init_array : > BOOT
.emb_text : > BOOT
.cert_element : > FLASH_CERT
.fnPtr : > FLASH_FNPTR
.ccfg : > FLASH_CCFG (HIGH)
.vtable : > SRAM
.vtable_ram : > SRAM
vtable_ram : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
.nonretenvar : > SRAM
.gpram : > GPRAM
}
And this is the linker file of the pwm led example:
/*
* Copyright (c) 2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== CC26X2R1_LAUNCHXL_NoRTOS.cmd ========
*/
--stack_size=1024 /* C stack is also used for ISR stack */
--heap_size=256
/* Retain interrupt vector table variable */
--retain=g_pfnVectors
/* Override default entry point. */
--entry_point main
/* Allow main() to take args */
--args 0x8
/* Suppress warnings and errors: */
/* - 10063: Warning about entry point not being _c_int00 */
/* - 16011, 16012: 8-byte alignment errors. Observed when linking in object */
/* files compiled using Keil (ARM compiler) */
--diag_suppress=10063,16011,16012
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */
/* The starting address of the application. Normally the interrupt vectors */
/* must be located at the beginning of the application. */
#define FLASH_BASE 0x0
#define FLASH_SIZE 0x58000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x14000
#define GPRAM_BASE 0x11000000
#define GPRAM_SIZE 0x2000
#define FLASH_START FLASH_BASE
#define PAGE_SIZE 0x2000
#define BOOT_BASE 0x50000
#define BOOT_END CERT_START - 1
#define BOOT_SIZE ((BOOT_END) - (BOOT_BASE) + 1)
#define APP_BASE 0x0
#define APP_END BOOT_BASE
#define APP_SIZE BOOT_BASE
#define FLASH_CCFG_START 0x00057FA8
#define FLASH_CCFG_END (FLASH_START + FLASH_SIZE - 1)
#define FLASH_CCFG_SIZE ((FLASH_CCFG_END) - (FLASH_CCFG_START) + 1)
#define FLASH_FNPTR_START FLASH_CCFG_START - 8
#define FLASH_FNPTR_END FLASH_FNPTR_START + 3
#define FLASH_FNPTR_SIZE 4
#define CERT_END FLASH_FNPTR_START - 1
#define CERT_SIZE 0x4C
#define CERT_START CERT_END - CERT_SIZE + 1
/* System memory map */
MEMORY
{
APP (RWX) : origin = APP_BASE, length = APP_SIZE
FLASH_CCFG (RX) : origin = FLASH_CCFG_START, length = FLASH_CCFG_SIZE
/* Application uses internal RAM for data */
SRAM (RWX) : origin = RAM_BASE, length = RAM_SIZE
/* Application can use GPRAM region as RAM if cache is disabled in the CCFG
(DEFAULT_CCFG_SIZE_AND_DIS_FLAGS.SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM = 0) */
GPRAM (RWX): origin = GPRAM_BASE, length = GPRAM_SIZE
}
/* Section allocation in memory */
SECTIONS
{
.intvecs : > APP_BASE
.text : > APP
.TI.ramfunc : {} load=FLASH, run=SRAM, table(BINIT)
.const : > APP
.constdata : > APP
.rodata : > APP
.binit : > APP
.cinit : > APP
.pinit : > APP
.init_array : > APP
.emb_text : > APP
.ccfg : > FLASH_CCFG (HIGH), TYPE=NOLOAD
.vtable : > SRAM
.vtable_ram : > SRAM
vtable_ram : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
.nonretenvar : > SRAM
.gpram : > GPRAM
}