Part Number: EK-TM4C123GXL
Tool/software: Code Composer Studio
I am a new user, and I am trying to debug one of my programs. Allow me to quickly summarize my situation.
Originally, I wanted the LED to light up if value >= 1. This worked fine, for a while. Then, I made several changes to the functions above the main function. I made these changes in the Code::Blocks IDE, and when I compiled and ran these changes in Code::Blocks, everything was fine. However, when I tried porting these changes back to CCS, I found I could no longer light the LED, even if the argument of the if statement is 1==1, which should always return true no matter what. To me, this implies that there is something fundamentally wrong with the code or with a CCS setting.
How do I light up the LED again? It should be noted that the CCS code can compile, but when I try debugging it, the LED no longer lights up.
Attached is the code. The most important section is down in the main function.
Thank you for your time. Any help would be appreciated.
#include <stdio.h>
#include <stdlib.h>
#include <stdbool.h>
#include <stdint.h>
#include "driverlib/adc.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
uint8_t ui8PinData = 2;
// Creates data square wave (for testing purposes, for the real implementation actual ADC data will be used). This
// square wave has unity magnitude.
// The number of high values in each period is determined by high values = array size / (2 * number of pulses)
void createDataWave(uint16_t arraySize, uint8_t pulsesNumber, uint8_t wave[]){
uint8_t highValues = arraySize / (2 * pulsesNumber);
uint8_t counter = 0;
uint16_t p;
for(p = 0; p < arraySize; p++){
if ((counter % 2) == 0){
wave[p] = 1;
} else{
wave[p] = 0;
}
if ((p + 1) % highValues == 0){
counter++;
}
}
}
// Creates analyzing square wave. This square wave has unity (1) magnitude.
// The number of high values in each period is determined by high values = (analyzingT/2) / time increment
void createAnalyzingWave(uint16_t analyzingFreq, uint16_t dataFreq, uint16_t arraySize, uint8_t pulsesNumber, uint8_t wave[]){
uint8_t highValues = (1 / analyzingFreq) * 0.5 / ((pulsesNumber * (1 / dataFreq)) / arraySize);
uint8_t counter = 0;
uint16_t p;
for(p = 1; p <= arraySize; p++){
if ((counter % 2) == 0){
wave[p - 1] = 1;
} else{
wave[p - 1] = 0;
}
if (p % highValues == 0){
counter++;
}
}
}
// Multiply each array element with the respective element of the other
// array and add each product together. returns the product. This forms
// the basis of the cross-correlation process.
// Technically, this function only multiplies and adds arrays of size arraySize.
// array2 is the big analyzing wave.
uint16_t multiplyAdd(uint8_t array1[], uint8_t array2[], uint16_t arraySize, uint16_t bigArraySize){
uint8_t productArray[arraySize];
uint16_t i;
uint16_t stepper = bigArraySize - 1;
uint16_t sum = 0;
for(i = arraySize - 1; i >= 0; i--){
productArray[i] = array1[i] * array2[stepper];
sum = sum + productArray[i];
stepper--;
}
return sum;
}
// Circle shift array one element to the left. This forms the basis of the
// time-shifting operation of the cross-correlation.
// ArraySize MUST be calculated separately
void circleShiftL(uint8_t array[], uint16_t arraySize){
uint16_t lastArrayIndex = arraySize - 1;
uint8_t lastElement = array[lastArrayIndex];
uint16_t j;
for(j = lastArrayIndex; j > 0 ; j--){
array[j] = array[j - 1];
}
array[0] = lastElement;
}
// Averages the array with the maximum correlation values
uint16_t arrayAverage(uint16_t array[], uint16_t arraySize){
uint16_t i;
uint16_t sum = 0;
//double average;
for(i = 0; i < arraySize; i++){
sum = array[i] + sum;
}
//average = sum / arraySize;
return sum / arraySize;
}
// Cross-correlate two arrays with each other. Returns the maximum cross-correlation value.
// Array size of each array must be specified.
uint16_t crossCorrelationV2(uint8_t dataWave[], uint8_t analyzingWave[], uint16_t arraySize){
uint16_t bigArraySize = (2 * arraySize) - 1;
// Expand analyzing array into array of size 2arraySize-1
uint8_t bigAnalyzingArray[bigArraySize];
uint16_t i;
// Set first few elements of the array equal to analyzingWave
// Set remainder of big analyzing array to 0
for(i = 0; i < arraySize; i++){
bigAnalyzingArray[i] = analyzingWave[i];
bigAnalyzingArray[i + arraySize] = 0;
}
uint16_t maxCorrelationValue = 0;
uint16_t currentCorrelationValue;
for (i = 0; i < bigArraySize; i++){
currentCorrelationValue = multiplyAdd(dataWave, bigAnalyzingArray, arraySize, bigArraySize);
if (currentCorrelationValue > maxCorrelationValue){
maxCorrelationValue = currentCorrelationValue;
}
circleShiftL(bigAnalyzingArray, bigArraySize);
}
return maxCorrelationValue;
}
int main(){
// Enables the clock
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
// Enables pin F
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
// Enables the output LEDs
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
uint16_t dataFreq = 1300;
uint16_t analyzingFreq = 1300;
uint16_t arraySize = 64;
uint8_t pulsesNumber = 16;
uint8_t analyzingWave[arraySize];
uint8_t dataWave[arraySize];
createAnalyzingWave(analyzingFreq, dataFreq, arraySize, pulsesNumber, analyzingWave);
createDataWave(arraySize, pulsesNumber, dataWave);
uint16_t value = crossCorrelationV2(dataWave, analyzingWave, arraySize);
while (1){
if(1==1){
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, ui8PinData);
} else {
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x00);
}
SysCtlDelay(2000000);
}
}