Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hello all,
I'm new on MCU programming so please bear with me :) My original idea was to control 5 servo motors via keyboard.
So, firstly I have checked if I'm able to set up all available PWM outputs on TM4C123G launchpad and surprisingly I was :) I've made code that all 16 PWM would work "simultaneously" with this code:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "inc/hw_gpio.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/pwm.h"
#include "driverlib/sysctl.h"
int main(void)
{
//System clock set up
SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
//Enable peripherals
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//Enable PWM modules
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
//Unlock PortF PIN_1
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
//Configure PWM pins
GPIOPinConfigure(GPIO_PB6_M0PWM0);
GPIOPinConfigure(GPIO_PB7_M0PWM1);
GPIOPinConfigure(GPIO_PB4_M0PWM2);
GPIOPinConfigure(GPIO_PB5_M0PWM3);
GPIOPinConfigure(GPIO_PE4_M0PWM4);
GPIOPinConfigure(GPIO_PE5_M0PWM5);
GPIOPinConfigure(GPIO_PC4_M0PWM6);
GPIOPinConfigure(GPIO_PC5_M0PWM7);
GPIOPinConfigure(GPIO_PD0_M1PWM0);
GPIOPinConfigure(GPIO_PD1_M1PWM1);
GPIOPinConfigure(GPIO_PA6_M1PWM2);
GPIOPinConfigure(GPIO_PA7_M1PWM3);
GPIOPinConfigure(GPIO_PF0_M1PWM4);
GPIOPinConfigure(GPIO_PF1_M1PWM5);
GPIOPinConfigure(GPIO_PF2_M1PWM6);
GPIOPinConfigure(GPIO_PF3_M1PWM7);
//Set pins type
GPIOPinTypePWM(GPIO_PORTA_BASE, GPIO_PIN_6 | GPIO_PIN_7);
GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);
GPIOPinTypePWM(GPIO_PORTC_BASE, GPIO_PIN_4 | GPIO_PIN_5);
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1);
GPIOPinTypePWM(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
//Configure PWM generators
PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM1_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM1_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM0_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM0_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM0_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM0_BASE, PWM_GEN_3, PWM_GEN_MODE_DOWN);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, 4095);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_1, 4095);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, 4095);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_3, 4095);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_0, 4095);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_1, 4095);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_2, 4095);
PWMGenPeriodSet(PWM0_BASE, PWM_GEN_3, 4095);
//Enable PWM generators
PWMGenEnable(PWM1_BASE, PWM_GEN_0);
PWMGenEnable(PWM1_BASE, PWM_GEN_1);
PWMGenEnable(PWM1_BASE, PWM_GEN_2);
PWMGenEnable(PWM1_BASE, PWM_GEN_3);
PWMGenEnable(PWM0_BASE, PWM_GEN_0);
PWMGenEnable(PWM0_BASE, PWM_GEN_1);
PWMGenEnable(PWM0_BASE, PWM_GEN_2);
PWMGenEnable(PWM0_BASE, PWM_GEN_3);
//Set PWM outptus state
PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT | PWM_OUT_1_BIT | PWM_OUT_2_BIT | PWM_OUT_3_BIT | PWM_OUT_4_BIT | PWM_OUT_5_BIT | PWM_OUT_6_BIT | PWM_OUT_7_BIT, true);
PWMOutputState(PWM0_BASE, PWM_OUT_1_BIT | PWM_OUT_1_BIT | PWM_OUT_2_BIT | PWM_OUT_3_BIT | PWM_OUT_4_BIT | PWM_OUT_5_BIT | PWM_OUT_6_BIT | PWM_OUT_7_BIT, true);
while (1)
{
//Rotation clockwise
uint32_t speed = 100;
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_1, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_3, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_5, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_6, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_7, speed);
SysCtlDelay(SysCtlClockGet() * 2);
//Rotation counter-clockwise
speed = 2100;
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_0, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_1, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_2, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_3, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_4, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_5, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_6, speed);
PWMPulseWidthSet(PWM0_BASE, PWM_OUT_7, speed);
SysCtlDelay(SysCtlClockGet() * 2);
}
}
Then, I tried to set up UART communication with my PC via Tera Term terminal and control 5 servo motors with keyboard buttons 0,1,2,3,4 for one counter-clockwise rotation and 5,6,7,8,9 for clockwise rotation and "s" for stopping with code below, but unfortunately only 0,1,2 and 5,6,7 seems working (motor is rotating depending on push of button) for pins PD0, PD1 and PA6. Maybe someone could help solve this mystery, why other 4 buttons (3,4 & 8,9) is not starting my servo motor?
#include<stdint.h>
#include<stdbool.h>
#include"inc/hw_memmap.h"
#include"inc/hw_types.h"
#include"inc/hw_gpio.h"
#include"driverlib/gpio.h"
#include"driverlib/pin_map.h"
#include"driverlib/pwm.h"
#include"driverlib/sysctl.h"
#include "driverlib/uart.h"
//MAIN FUNCTION
int main(void)
{
unsigned char button;
volatile uint32_t speed; //VARIABLE FOR PWM_WIDTH SET AS % FROM 0 TO 100
//CLOCK SETTINGS - SET SYSTEM CLOCK TO 40MHz
SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
//SET PWM CLOCK AS SYSTEM CLOCK DIVIDED BY 64
SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
//ENABLE PERIHPERALS
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
//Enable PWM
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
//CONFIGURE PINS
GPIOPinConfigure(GPIO_PD0_M1PWM0);
GPIOPinConfigure(GPIO_PD1_M1PWM1);
GPIOPinConfigure(GPIO_PA6_M1PWM2);
GPIOPinConfigure(GPIO_PA7_M1PWM3);
GPIOPinConfigure(GPIO_PF1_M1PWM5);
//SET PINS TYPE FOR PWM
GPIOPinTypePWM(GPIO_PORTA_BASE, GPIO_PIN_6 | GPIO_PIN_7);
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_1);
//CONFIGURE PWM GENERATOR
PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM1_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_DOWN);
//SET PWM GENERATORS WITH MODE OF OPERATION AS COUNTING
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, 4095);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_1, 4095);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, 4095);
//Enable PWM generators
PWMGenEnable(PWM1_BASE, PWM_GEN_0);
PWMGenEnable(PWM1_BASE, PWM_GEN_1);
PWMGenEnable(PWM1_BASE, PWM_GEN_2);
//Set PWM outputs state
PWMOutputState(PWM1_BASE, PWM_OUT_0 | PWM_OUT_1 | PWM_OUT_2 | PWM_OUT_3 | PWM_OUT_4 | PWM_OUT_5 | PWM_OUT_6 | PWM_OUT_7, true);
//Set up UART communication
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//CONFIGURE UART, BAUD RATE 9600, DATA BITS 8, STOP BIT 1, PARITY NONE
UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 9600, (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
while (1)
{
speed = 100;
if (UARTCharsAvail(UART0_BASE))
{
button = UARTCharGet(UART0_BASE);
}
else
{
button = 100;
}
if (button == '0')
{
speed = 100; //ROTATION COUNTER-CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, speed); //SET THE PULSE WIDTH
}
if (button == '1')
{
speed = 100; //ROTATION COUNTER-CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, speed); //SET THE PULSE WIDTH
}
if (button == '2')
{
speed = 100; //ROTATION COUNTER-CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, speed); //SET THE PULSE WIDTH
}
if (button == '3')
{
speed = 100; //ROTATION COUNTER-CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, speed); //SET THE PULSE WIDTH
}
if (button == '4')
{
speed = 100; //ROTATION COUNTER-CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, speed); //SET THE PULSE WIDTH
}
if (button == '5')
{
speed = 2100; //ROTATION CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, speed); //SET THE PULSE WIDTH
}
if (button == '6')
{
speed = 2100; //ROTATION CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, speed); //SET THE PULSE WIDTH
}
if (button == '7')
{
speed = 2100; //ROTATION CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, speed); //SET THE PULSE WIDTH
}
if (button == '8')
{
speed = 2100; //ROTATION CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, speed); //SET THE PULSE WIDTH
}
if (button == '9')
{
speed = 2100; //ROTATION CLOCKWISE
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, speed); //SET THE PULSE WIDTH
}
if (button == 's')
{
speed = 0; //NO ROTATION
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6, speed);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_7, speed);
}
SysCtlDelay(SysCtlClockGet() / 90);
}
}