Part Number: EK-TM4C1294XL
Hello everybody,
We are trying to upgrade an old S12 based controller used in poultry farms with the EK-TM4C1294XL.
One of the key factors for the development is the capability of retaining RTC data during power failures lasting few minutes to few hours.
We are trying to figure out if this can be achieved by removing R39 and provide separate power to TP11 (3,3V-main power or 3V-lithium battery), without enabling hibernation mode.
The three main questions that arise are:
Q1 Will the RTC powered by the battery retain the RT data?
Q2 What is the consumption of the internal circuitry powered from VBAT pin?
Q2 After the main power return, is there a need of RTC data synchronization or the transition from battery(3V) to main power (3,3V) will be transparent as desired ?
Thank you in advance!