Other Parts Discussed in Thread: AM3356
Hi,
My requirement is to use the uniflash tool in the production environment to flash the AM3356 based custom board.
I went through below link ,
it was mention that we can use the command line to flash the board through uniflash and as support uniflash has provided the Flash writer bin file for only selected board.
As per our understand, if we able to load the flash writer bin file through JTAG (xds200), then we can load the MLO, uboot and kernel image to the board.
but, the flash writer bin file provided with uniflash will not support my custom board, So need help on how to proceed further.
http://software-dl.ti.com/processor-sdk-rtos/esd/docs/latest/rtos/index_board.html#uniflash