Other Parts Discussed in Thread: MSP430FR2355
Hi, there!
We're very interested in TI's dual ray/wave technique used in smoke detector development.
Now, we are evaluating MSP430FR2355, for we've read the excellent application report SLAA930.
The test result section on p.14 section 5.1 really got our attention!
We'd like to know further about the test result:
What part is the photo-diode?!
I suppose the photo-diode need to have a sensitivity range down to, say 500nm?
Also, I've noticed that in TPS8804EVM, blue led and photo-diode listed in BOM are SFH123 and LTL1CHTBK4.
The latter blue led has 470nm wavelength, however the photo-diode has spectrum from 700nm to 1100nm.
It seems that he photo-diode simply can't receive any scattered blue light, right?
Thanks for reading this post.
Zt.