Part Number: TM4C129ENCPDT
i am using the NDK for TCP/IP over ethernet i had been able to configure the static IP to my device using the XCONFIG , the program works fine the issue that i have is i need to change the Static IP , when the controller receives a new Static IP while running ( i dont mind rebooting if there is no other way). how can this be done??
as per my understanding the IP configuration takes place in ti_ndk_config_Global_stackThread which run as soon as the system boots so i cant do any thing on it.