Part Number: RM46L852
Tool/software: Code Composer Studio
Hi Team,
I am facing a problem with SCI communication. I have interfaced Nextion Display to LIN Interface. RX Interrupt is not working and I am not able to recieve anything from Display. I can transmit to display from controller. I created one button in Nextion HMI (UART) and when I click it , display will send ID, which I want to recieve from controller. But I am not able to recieve. Please help
Settings I made are:
1. SCI2 driver
2. RX INT
3. VIM Channel 13 Enabled
Code is attached.
/** @file sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
#include "system.h"
#include "sci.h"
#include "string.h"
#include "stdio.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
static unsigned char command;
uint8 frame[100]={};
uint8 frame1[100]={};
uint8 recieveframe[100]={};
uint8 len,len1;
uint8 rlen;
int i,j=0;
int reciveflag;
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
len=0;
reciveflag=0;
rlen=0;
_enable_IRQ();
sciInit();
sciEnableNotification(scilinREG,SCI_RX_INT);
sciReceive(scilinREG,7,(unsigned char *)&recieveframe);
while(1)
{
// sciReceive(scilinREG,1,(unsigned char *)&recieveframe);
}
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
void sciNotification(sciBASE_t *sci, uint32 flags)
{
/* enter user code between the USER CODE BEGIN and USER CODE END. */
/* USER CODE BEGIN (29) */
// sciReceive(scilinREG,rlen,(unsigned char *)&recieveframe);
}
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
len=0;
reciveflag=0;
rlen=0;
_enable_IRQ();
sciInit();
sciEnableNotification(scilinREG,SCI_RX_INT);
sciReceive(scilinREG,7,(unsigned char *)&recieveframe);
while(1)
{
// sciReceive(scilinREG,1,(unsigned char *)&recieveframe);
}
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
void sciNotification(sciBASE_t *sci, uint32 flags)
{
/* enter user code between the USER CODE BEGIN and USER CODE END. */
/* USER CODE BEGIN (29) */
// sciReceive(scilinREG,rlen,(unsigned char *)&recieveframe);
}
/* USER CODE END */