This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Two Microcntrollers on board: one or two crystals for good EMI test?

Good morning,

i'm developing a design with two uCs that run at 8or 16 MHz, and I must choice if use a single crystal with OSC_OUT_1 to OSC_IN_2 or two separate crystals and no connection between uCs: what is the best solution for EMI tests, also keeping in mind that componenst vould be at 3 or 4 centimeters in distance?

Thank you in advence for help!!!

Fabio