Part Number: TMS570LS0432
Tool/software: TI C/C++ Compiler
Hello
I do the two cpu with spi commnunication ,master,and slave
but in slave cpu ,I use api function spiGetData,means,but cpu can't interrupt
spi->INT0 |= 0x0100U; CPU can't do interrupt function< void mibspi1HighLevelInterrupt(void)>\
but I use api function spiSendAndGetData means spi->INT0 |= 0x0300U; cpu can do interrupt
why??
#pragma INTERRUPT(mibspi1HighLevelInterrupt, IRQ)
/* SourceId : SPI_SourceId_021 */
/* DesignId : SPI_DesignId_016 */
/* Requirements : HL_SR141, HL_SR142, HL_SR143 */
void mibspi1HighLevelInterrupt(void)