Part Number: TMS570LC4357
Tool/software: Code Composer Studio
hello,
I start up with TMS570LC43x launchpad and with the help of halogen I enable the gpio pin and then important the whole file to ccs7
and build the file with warning #112-D statement is unreachable
but when debug process is not executing as I received this error:
IcePick: Error connecting to the target: (Error -600 @ 0x0) A required dynamic library could not be located. The library isn't on the search path. (Emulation package 7.0.100.1)
so what should I do ,I also install XDS Emulation Software (EMUPack) Download 7.0.100.1
need guidance