Part Number: TM4C129ENCPDT
While researching the Hibernate module, Tamper module, and Real Time Clock, I discovered that the Hibernate module cannot be enabled without some sort of clock source on the XOSC0 pin.
The symptom is that _HibernateWriteComplete() locks up, waiting for HIB_CTL_WRC to be set, but that never occurs.
Note that I've been able to confirm that the Tamper module can detect failure of a crystal-based RTC source, but it doens't seem possible to detect failure during a cold boot. It would seem that some additional setup is needed before calling HibernateEnableExpClk(), besides the obvious SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE) and SysCtlPeripherReady(SYSCTL_PERIPH_HIBERNATE) wait.
Also, I tried rewriting _HibernateWriteComplete() to allow a 1.5-second (1500 ms) timeout, after which SysCtlPeripheralReset(SYSCTL_PERIPH_HIBERNATE) is called before repeating the Enable() and Ready() calls again. The peripheral reset, inspired by HIB#19, does not seem to help in the case where there is no crystal or other clock input on XOSC0.