Part Number: TM4C123GH6PZ
Hi TI:
When i debug TM4C123GH6PZ,sometimes the chip enter abort() function;
I know there is some problem with the code, how can i trace back to the line of code with error?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123GH6PZ
Hi TI:
When i debug TM4C123GH6PZ,sometimes the chip enter abort() function;
I know there is some problem with the code, how can i trace back to the line of code with error?
Thanks
Typically this fault occurs when you write to a peripheral for which you have not yet enabled the clocks. Often C stepping through your source code will help you identify which peripheral that is. For more details on diagnosing bus faults see:
Greetings,
Yao Aili said:how can I trace back to the line of code with error?
Depending upon the extent & complexity of your code - often it proves helpful to, "Divide your code into multiple, smaller sized sections." You then "independently" run & test (again only one) of each of these sections at a time. The reduced size of these "code sections" enables you to most always, "Speed, Ease & Enhance" your "traced-back detection" of the problem!
You should seek to confine your "sections" to complete code-blocks (multiple code-blocks are possible) - so that each section includes that necessary to execute properly.
It is my firm's (proven) belief that code should be developed in small/methodical "blocks" - with each block being individually tested & verified - prior to being, "Integrated w/in the general program. This progressive, code development method is noted as, "KISS" - and for decades has proven immensely empowering. (even though - especially though - "KISS" never is credited (nor sees the "light of day") here...)
After you've identified the "problem section" (hopefully just one section) the vendor's "MCU-centric" guidance should provide high/specific code detail - made far more efficient due to the, "Reduction in Code Size being "specific tested."
Reducing an issue's, "Size & Scope" (KISS) proves a classic method to, "Greatly Enhance Diagnostic Success!"