This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1237E6PM: Is the internal Flash memory NOR or NAND based?

Part Number: TM4C1237E6PM


If the internal Flash memory is NOR based, then it should be defect-free.  If it is NAND-based, then error detection and correction is more of an issue.  I think it is NOR-based because that is typical for internal flash in a micro, but I can't verify that in any of the documentation.