Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294KCPDT: About Vin_GPIO

Part Number: TM4C1294KCPDT

The datasheet states the absolute maximum rating of input voltage (Vin_GPIO) is 4V, (not VDD+**V), in table 27-1.

 

Does it mean situation like instantaneous voltage below 4V was applied to I/O ports before power was supplied to the micro controller is acceptable?  

Also, does this Vin_GPIO include input/output ports which are not set as GPIO (ex. AD port)?

  • Remember that absolute maximum is the value which exceeded may cause permanent damage to the part. The part will likely not operate properly at those levels. 

    Kurumi Hasegawa said:
    Does it mean situation like instantaneous voltage below 4V was applied to I/O ports before power was supplied to the micro controller is acceptable?

    You must also be below the absolute maximum current for that pin to be sure damage does not occur. I would not say acceptable because the device may be powered through the GPIO pin and its operation would be erratic. 

    Kurumi Hasegawa said:
    Also, does this Vin_GPIO include input/output ports which are not set as GPIO (ex. AD port)?

    Yes, but again this does not imply proper operation.

  • Hi, thank you a lot for the reply.

    So, is it OK (or will not break the device) to apply voltage below 4V to GPIO pin without supply voltage?

    I mean, usually voltage rating is described as VDD + xV, but for this device it is described as 4V (fixed value).

    It bugs me a little.

    Sincerely,

    Kurumi Hasegawa

  • I cannot say "OK", I can merely repeat what is in the datasheet: "The maximum ratings are the limits to which the device can be subjected without permanently damaging the device. Device reliability may be adversely affected by exposure to absolute-maximum ratings for extended periods."

  • I understand. Thank you a lot