Part Number: TMS570LS1224
Tool/software: Code Composer Studio
Hello, I have exactly the same issue as PL, driving the Rx pin on Launchpad (J6.3) from PC (FTDI 3.3V adapter), the pin is not pulled down to 0V but to 2.3V. If I look to the FTDI alone, the signal is pulled down to 0V. If I connect Launpad Rx/Tx together (loopback) and I transmit on Tx, Rx is pulled down to 0V!
I don't undertsand what is wrong ....