Part Number: TMS570LC4357-EP
Hello,
The TMS570 has a single EPWMSYNCO pin which can be driven by the EPWM module. That pin can be muxed to one several balls on the physical device with the IOMM. I'm wondering if it is possible to configure the IOMM to drive more than one ball with the same signal. That is, can I have the EPWM module drive a EPWMSYNCO signal which is routed to several places, effectively allowing me to coordinate the same SYNC signal to several external different devices. Thanks.