This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Shutdown MCU using a command

Part Number: TMS570LS1224

Hello,

I need to run a test in which the MCU is programmed to communicate through SPI/UART to configure another one of my devices and then after this send the MCU itself to shutdown/turn off using an instruction on the program, but without removing the power. The reason for this is because I need to configure my 2nd device with the MCU and then shutdown the MCU to be able to measure the noise radiated by my 2nd device. 

Because of the way this board was design (with both the MCU and the 2nd device in the same board and supplied by the same LDOs) if I remove the supply from the MCU I would also be shutting down the 2nd device. 

So, in summary, I want to know if there is another way of turning off the MCU other than removing the power. 

Best regards,

Leslie