Part Number: TMS570LC4357
Tool/software: Code Composer Studio
As part of the investigation into the related question about trying to rebuild the GNU ARM toolchain to add big-endian run time libraries to support the TMS570LC4357 device noticed some discrepancies about if this Cortex-R5F device is "BE8" or "BE32":
1. The TMS570LC4357 datasheet says "This device is BE32, or word invariant big endian".
2. When a new project is created for a TMS570LC4357 in CCS 10 using the TI compiler in the project properties under General -> Project type and tool chain -> Device endianness is "be32".
3. Yet, when the CCS debugger is attached to a TMS570LC4357 using a XDS110 the Target Status view reports "BE8", rather than "BE32":
4. Based upon the above Target Status I went to look at the ARM Cortex-R documentation to try and find which status bits indicate if the device is "BE8" or "BE32".
However, according to the Cortex-R5 Technical Reference Manual :
The processor supports byte-invariant big-endianness BE-8 and little-endianness LE. The processor does not support word-invariant big-endianness BE-32.
Given the above from the ARM Cortex-R4 Technical Reference Manual about a Cortex-R5 not supporting BE32, I am now not sure which of the conflicting information is correct.
Is there a bug in the CCS target status, or have I misunderstood the documentation?