Part Number: TMS570LS1114
Dear support team,
I just came across the following note, considering the CAN TX / RX signals in the technical reference manual for the Hercules MCU.
Note: When CAN_RX pin is connected to a CAN transceiver, an external pullup resistor has to be
used to ensure that the CAN bus will not be disturbed (for example, while the DCAN module is
reset).
Same note goes for the CAN_RX pin.
I just wanted to understand, why these resistors have to be added, when there exists already internal pullup resistors in the MCU itself against disturbances? I am especially interested in the reason to add this external resistor for the RX line.
Thank you and kind regards
Sebastian