Other Parts Discussed in Thread: UNIFLASH
Hi,
Since Uniflash version 5.3.0 we have been experiencing intermittent errors when loading our program onto our board. We are using DSLite to flash the board.
Our board is a TMS570LC43X CORTEX-R5 Microcontroller
XDS110 Emulator v9.1.0.00001
Uniflash 5.3.1.2265
The error is shown below:
For more details and examples, please refer to the UniFlash Quick Start guide
DSLite version 10.0.0.1942
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: IcePick
Executing Startup Scripts: IcePick
Initializing: Dap
Executing Startup Scripts: Dap
Initializing: CortexR5
Executing Startup Scripts: CortexR5
Connecting...
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0Loading Program: Multiple Files
Preparing ...
fatal: CortexR5: Error: (Error -1141 @ 0x1FE) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
text: 0 of 252 at 0x4000
fatal: CortexR5: Failed CPU Reset: (Error -1141 @ 0x1FE) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
error: CortexR5: File Loader: Memory write failed: CPU Reset error. Error code -1
Finished
Reloading the program to the board generates this error:
For more details and examples, please refer to the UniFlash Quick Start guide.
DSLite version 10.0.0.1942
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: IcePick
Executing Startup Scripts: IcePick
Initializing: Dap
Executing Startup Scripts: Dap
Initializing: CortexR5
Executing Startup Scripts: CortexR5
Connecting...
fatal: IcePick: Error connecting to the target: (Error -267 @ 0x0) The controller could not detect valid target supply. Check target JTAG connection and/or connection setting specifying voltage level. (Emulation package 8.4.0.00006)
Sometimes, multiple board power cycles are needed to bypass this error.
Is this a known issue with the Uniflash software?
Regards,
David