This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT: Uniflash serial interface

Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: UNIFLASH,

Dear TI-team,

i am using a custom bord with a TM4C129ENCPDT. I was used to flash my µC with the Segger Jlink. After that a bootloader was added to be able to flash over a serial(UART) interfave using the LM Flash Programmer. Since there is no Linux build i want to use Uniflash desktop but there is no option to select a serial port. So i wanted to ask, if there is a way to use the Uniflash CLI to flash a TM4C129ENCPDT over a serial port?

Thanks in advance,

Lukas