Dear Hercules Support Team,
In Table 6-46 in the TMS570LC4357 Datasheet there are several different parity errors mentioned fort he L2RAMW and the L2FMC (marked in the image). There seems to be little information in the documentation about the control and command parity.

If I understand correctly the control parity is the parity for the control bus, but I can’t find any information on the command parity and the „command parity error on idle“:
Q1: What is the command parity and why is there only a „command parity error on idle“?
Q2: Is the L2FMC „Mcmd parity error on Idle command“ the same as the L2RAMW „command parity error on idle“, but for the L2FMC?
Q3: Is the L2FMC „internal parity error“ the same as a control parity error?
Thanks in advance and best regards,
Max