This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS570LC4357: SafeTI Library TAU with LDRA unit Ti Qual 9.8.3 Compile Issue

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Tool/software: TI C/C++ Compiler

we have some issue with the new version of the LDRA unit TI Qual (9.8.3) when working with the SafeTI TAU. 

We get compile errors from undefined symbols (e.g: QQQindicator  , qqqupload , qqzzglobarrb  , etc.)   resulting from LDRA instrumentation,which was not something that occurred when we tried running the demo application, which was a 9.4.3 LDRA unit TI Qual release. 

We are currently just setting up and testing with the demo_app on the lc4357 devkit.

Is there anything else to modify in the configuration when using the SafeTI TAU with 9.8.3  as compared to 9.4.3.

Thanks in advance