This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS0714: Active Cell Balancing is not working

Part Number: TMS570LS0714

Tool/software: Code Composer Studio

Dear Sir,

We are performing Active cell balancing algorithm in TMS570Ls0714 PCB board. When we are debugging code,  g_ui32EMB1428Status is giving error of 0x80. than We went through  of  EMB1428 datasheet. Active cell balancing is working in Evolution board ,  g_ui32EMB1428Status is giving 0xA9 during discharging of Cell 1. with 0xA0 which indicates no error.  But in our case, First time g_ui32EMB1428Status is giving 0xA9 during discharging of Cell 1 with 0x80 which indicates CS falling edge while the EMB1428 is still waiting for a transition on DONE (rising or falling edge). 

than continuously this error is indicating.

How to resolve this error? Can you please give us suggestion.

it is urgent requirement..

Thanks and regards,

Krunal Desai