Part Number: TM4C1290NCPDT
TI Friends & Family,
Our customer is doing some work on a steering controller. They want to be able to time the A/B pulses coming into the system through the hardware QEI interface on a TI TM4C1290PDT controller. They can get counts, velocity and everything else needed to report but there is no obvious way to interrupt on line changes. They understand they can with GPIOs as they actually do it to handle a second encoder. Their thought is once they have enabled the special QEI mode on the pins, GPIO like handling is lost.
So, regarding the QEI on the 1290PDT is this possible? They are mostly looking for an estimate for firmware to support this and it may not be possible to do without a hardware change in fact. But any comments or guidance is certainly welcomed.
Thank you and Viva La Tiva!
-Chris