There are numerous errors in the CRC section (22) of the TRM. Here is a list of the ones I have spotted so far:
The register offsets in section 22.5 bear little resemblance to the offsets in the detailed descriptions from section 22.5.1 onwards. I assume the ones in the detailed sections are correct?
Section 22.5 says that CRC_INTR and CRC_STATUS are at the same register address offset (both at 0x34 which is a bit unlikely I think!).
Section 22.5.22 has the heading CRC Pattern Counter Preload Register 1 but the register name in brackets is CRC_PCOUNT_REG2
None of the hyperlinks (i.e. the page numbers) in section 22.5 work.
Regards,
Richard