Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN, ADS1278
Tool/software: Code Composer Studio
Hello,
In my project, I want to generate PWM Signal of 4 channel.
1. PWM Channel 1 ==> I need to generate 10MHz clock.
2. PWM Channel 2 ==> I need to generate 6KHz clock.
3. PWM Channel 3 ==> I need to generate 1KHz clock.
4. PWM Channel 4 ==> I need to generate 500Hz clock.
3 Input Capture signal need to configure.
Above configuration i tried with RM48L952 board, except PWM channel 1,remaining PWM channels output i can achieve using HALCogen code generation software.
using HALCogen software i can reach maximum upto ~1MHz.
But, in my application i need to get 10MHz of clock which i need to connect with ADS1278.
I have viewed TI forum, i can understood that for better and more frequency generation better to go with HET IDE.
I installed the HET IDE, i dont know how to configure and import that things my project.Can you please guide me how to
make the above configuration to achieve....
if possible kindly share me the code with those configuration. It helpful for me....
Reply me soon as possible......
Regards,
Anand Kumar