Other Parts Discussed in Thread: TMS570LS20216, NOWECC, HALCOGEN
Hi,
I am using the TMS570 Microcontroller Development Stick, with a TMS570LS20216 MCU (ASPGEQQ1). I would like to be able to use a timer, such as timer 0 to generate regular interrupt ticks, that can be used to perform time critical tasks.
I have used timer 0 previously on a project using a TMS320, which used the interrupt _c_int99. I have looked at the code that comes with the development stick, which mentions timer 0. But the only reference to timer 0 is as follows:
/* Timer 0 Configuration */
/* 0x44 */
union t0c
{
unsigned long T0C_UL;
struct
{
unsigned : 2;
unsigned t0mo_B14 : 14;
unsigned : 1;
unsigned t0cc_B7 : 7;
unsigned : 6;
unsigned t0ms_B1 : 1;
unsigned t0rc_B1 : 1;
} T0C_ST;
} T0C_UN;
Can I use this timer to generate regular interrupts?
Is there any sample code available that could help me generate regular timer interrupts using timer 0 or any other timer?
Or can anyone point me in the right direction?
Regards,
Dave