Hello guys,
I have a problem with my interrupt within the TMS570. I am working with the MCBTMS570 and CCSv4.
I programmed a RTI based blinking LED a while ago. Everything worked fine.
Afterwards I tried to get the CAN working. The CAN should work interrupt based too. In debug mode I could see the correct adress of the ISR in the register IRQVECREG. But the ISR was not running. Then I switched back to my blinkig LED program and now this one is not running either.
Do I miss something???
EDIT:
Problem solved. I forgot the global interrupt enable. But I could have sworn the original blinking LED had worked without this.