Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL2-RM46: ADC DAC example: was this made for a board with external memory?

Part Number: LAUNCHXL2-RM46

I'm trying to build this example: ADC_DAC.zip.

It's for the RM46x. The following variables are declared in sys_main.c

uint32 adc1_EV_results[43200];
uint32 adc1_G1_results[43200];

and notification.c:

uint32    adc1_EV_results_copy[43200];
uint32    adc1_G1_results_copy[43200];

extern uint32 adc1_EV_results[43200];
extern uint32 adc1_G1_results[43200];

	int i = 0;

	if (channel == 0)
	{
		for (i=0; i<86400; i++)
		{
			adc1_EV_results_copy[i] = adc1_EV_results[i];
		}
	}
	else if (channel == 1)
	{
		for (i=0; i<86400; i++)
		{
			adc1_G1_results_copy[i] = adc1_G1_results[i];
		}

	}
	else
	{
		while(1);			// should never get here
	}


Why is the counter the double of the array lenghth?