Part Number: TM4C1294KCPDT
Hello Everyone,
In my application (NORTOS, lwip, TivaWare_C_Series-2.1.2.111) I am implementing web server in sd card that worked fine, also I checked data logging of data at defined interval (i.e. in seconds) in sd card which also worked for me.
But when I try to implement both the application in one project, then after some time i am unable to get data from sd card i.e. web browser shows error: "404: The Requested file cannot be found."
Also data logging to file not happened at that time.
When I tried to debug the project in ccs, at the time of 'f_open' function in 'fs_open' of html fs file, it gives me error "FR_NOT_READY" or "FR_DISK_ERR". Same errors are coming for data logging part.
Could any one suggest some example code for the same or some methods to implement this application..