This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0914: ADC-input-leakage

Part Number: TMS570LS0914

Hi E2E,

me and my team are using the ADCs for several voltage measurements and we want to determine the accuracy of our system based on component tolerances, leakages, etc.

The datasheet seems to show that the leakage current is equivalent to current sources parallel to the inputs:

Table 7-24 gives us a value for the leakage current which we should expect in our system:

Do these values refer to a certain range of values for Rext and Cext?

Do large values of Rext necessicarly lead to a larger error due to the leakage current beeing constant, regardless of source impedance at the input?

Is the leakage constant or does it change dependend on the source impedance?

Hope you can help us out.

Thanks and best regards,

David