Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
Hi,
I am using AUTOSAR_MCAL_TMS570LSx-05.40.00 package in my project.
I have configured NHET pins for ICU for PWM input signal measurement.
ICU driver reads the correct frequency and duty cycle, if the input frequency is above 100 Hz.
For frequencies lesser than 100Hz, duty cycle and frequency measured by ICU driver toggles between 0 and PWM input set value. This behavior is incorrect. Please provide a fix for this issue.